This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: CC2652R 使用协议栈 simplelink_cc13x2_26x2_sdk_4_40_04_04中 scan

Part Number: CC2652R

使用CC2652R,协议栈 simplelink_cc13x2_26x2_sdk_4_40_04_04,使用RTLS_aoa过程中,我修改了slave节点的广播名称(F8:8A:5E:2C:44:7E未修改,D0:2E:AB:2D:B2:22,D0:2E:AB:2D:AD:C3已修改),将RTLSSLAVE修改为MLSLAVE,采用rtls_ui开启扫描,结果依然可以扫到,这是什么原因?