Part Number: LAUNCHXL-CC26X2R1
Hi,
我现在有两块LAUNCHXL-CC26X2R1评估板A和B,修改了rtls_slave example代码,让A实现仅仅发送unconnectable unscanable undirect的 ble 5.0 extend periodic adv packet。
修改了simple_central example代码,参考 "ble5 stack user guide"实现了scan Synchronize with a periodic advertising train。但是问题是没有GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT上报,
即无法建立Periodic Advertising同步。
我简单介绍下我的环境:
step1:在ccs10的工程选项中添加了ARM Linker pre-define macro “”“USE_PERIODIC_SCAN”;
step2:初始化GAP_PROFILE_CENTRAL角色
static void SimpleCentral_init(void)
{
BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- init ", SC_TASK_PRIORITY);
// ******************************************************************
// N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
// ******************************************************************
// Register the current thread as an ICall dispatcher application
// so that the application can send and receive messages.
ICall_registerApp(&selfEntity, &syncEvent);
// Create an RTOS queue for message from profile to be sent to app.
appMsgQueue = Util_constructQueue(&appMsg);
GGS_AddService(GATT_ALL_SERVICES); // GAP
// Register with GAP for HCI/Host messages (for RSSI)
GAP_RegisterForMsgs(selfEntity);
BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- call GAP_DeviceInit", GAP_PROFILE_CENTRAL);
// Initialize GAP layer for Central role and register to receive GAP events
GAP_DeviceInit(GAP_PROFILE_CENTRAL, selfEntity, addrMode, &pRandomAddress);
dispHandle = Display_open(Display_Type_UART, NULL);
Display_printf(dispHandle, SC_ROW_SEPARATOR_1, 0, "====================");
}
step3:先设置scan参数,此时不发送scan_enable。然后发送
GapScan_PeriodicAdvCreateSync,其中sid以及广播设备地址已知直接指定
static void SimpleCentral_processGapMsg(gapEventHdr_t *pMsg)
{
switch (pMsg->opcode)
{
case GAP_DEVICE_INIT_DONE_EVENT:
{
uint8_t temp8;
uint16_t temp16;
gapDeviceInitDoneEvent_t *pPkt = (gapDeviceInitDoneEvent_t *)pMsg;
BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- got GAP_DEVICE_INIT_DONE_EVENT", 0);
// Setup scanning
// For more information, see the GAP section in the User's Guide:
// http://software-dl.ti.com/lprf/ble5stack-latest/
// Register callback to process Scanner events
GapScan_registerCb(SimpleCentral_scanCb, NULL);
// Set all Scanner Event Mask
GapScan_setEventMask(GAP_EVT_SCAN_EVT_MASK);
// Set Scan PHY parameters
GapScan_setPhyParams(SCANNED_PHY_1M, SCAN_TYPE_PASSIVE,
SCAN_PARAM_DFLT_INTERVAL , SCAN_PARAM_DFLT_WINDOW );
// Set all Advertising report fields to keep
temp16 = SCAN_PARAM_ALL_RPT_FIELDS;
GapScan_setParam(SCAN_PARAM_RPT_FIELDS, &temp16);
// Set Scanning Primary PHY
temp8 = SCANNED_PHY_1M;
GapScan_setParam(SCAN_PARAM_PRIM_PHYS, &temp8);
// Set LL Duplicate Filter
temp8 = SCAN_FLT_DUP_ENABLE;
GapScan_setParam(SCAN_PARAM_FLT_DUP, &temp8);
// Set PDU type filter -
// Only 'Connectable' and 'Complete' packets are desired.
// It doesn't matter if received packets are
// whether Scannable or Non-Scannable, whether Directed or Undirected,
// whether Scan_Rsp's or Advertisements, and whether Legacy or Extended.
//temp16 = SCAN_FLT_PDU_CONNECTABLE_ONLY | SCAN_FLT_PDU_COMPLETE_ONLY;
//temp16 = SCAN_FLT_PDU_EXTENDED_ONLY;
temp16 = SCAN_FLT_PDU_NONCONNECTABLE_ONLY;
BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- GapScan_setParam", 0);
GapScan_setParam(SCAN_PARAM_FLT_PDU_TYPE, &temp16);
#ifdef USE_PERIODIC_SCAN
// this is a periodic advertisement
GapScan_PeriodicAdvCreateSyncParams_t pSyncParams;
//uint8 t_addr[6]={0xCB,0x98,0x2D,0x5E,0x8A,0xF8};
pSyncParams.options = SCAN_PERIODIC_DO_NOT_USE_PERIODIC_ADV_LIST |
SCAN_PERIODIC_REPORTING_INITIALLY_DISABLED;
pSyncParams.advAddrType = ADDRTYPE_PUBLIC; // only ADDRTYPE_PUBLIC and ADDRTYPE_RANDOM are allowed
//osal_memcpy(pSyncParams.advAddress, t_addr, B_ADDR_LEN);
pSyncParams.advAddress[5] = 0xF8;
pSyncParams.advAddress[4] = 0x8A;
pSyncParams.advAddress[3] = 0x5E;
pSyncParams.advAddress[2] = 0x2D;
pSyncParams.advAddress[1] = 0x98;
pSyncParams.advAddress[0] = 0xCB;
pSyncParams.skip = 0; // should be between 0 and SCAN_PERIODIC_SKIP_MAX
pSyncParams.syncTimeout = 1000; // synchronization timeout for the periodic advertising train is 1000*10ms = 10s
// should be between SCAN_PERIODIC_TIMEOUT_MIN and SCAN_PERIODIC_TIMEOUT_MAX
pSyncParams.syncCteType = SCAN_PERIODIC_CTE_TYPE_ALL;
uint8_t status = GapScan_PeriodicAdvCreateSync(0x01, &pSyncParams);
Display_printf(dispHandle, SC_ROW_SCAN_3, 0, "PeriodicAdvCreateSync status! 0x%x",status);
#endif
break;
}
case GAP_SCAN_CREATE_SYNC_EVENT:
{
GapScan_PeriodicAdvEvt_t *pPkt = (GapScan_PeriodicAdvEvt_t *)pMsg;
uint8_t status;
Display_printf(dispHandle, SC_ROW_SCAN_EVT_5, 0, "GAP_SCAN_CREATE_SYNC_EVENT Status 0x%x",pPkt->status);
if(pPkt->status == SUCCESS)
{
status = GapScan_enable(0, 0, 0);
//if(SUCCESS != status)
{
Display_printf(dispHandle, SC_ROW_SCAN_EVT_2, 0, "GapScan_enable again status 0x%x",status);
}
}
}
break;
case GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT:
{
Display_printf(dispHandle, SC_ROW_SCAN_EVT_3, 0, "GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT");
}
break;
case GAP_SCAN_PERIODIC_ADV_SYNC_LOST_EVENT:
{
Display_printf(dispHandle, SC_ROW_SCAN_EVT_7, 0, "GAP_SCAN_PERIODIC_ADV_SYNC_LOST_EVENT");
}
break;
default:
break;
}
}
step4:生成GAP_SCAN_CREATE_SYNC_EVENT后,开启scan_enable
等待GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT。
现在就是GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT一直没有出现,我检查了代码、读了文档手册不知道问题出现在哪?请给予帮助,万分感谢