This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: CC2640R2F 使用手机APP 更新蓝牙连接参数时出现异常

Part Number: CC2640R2F

使用2个模块,一个购买,一个自制,购买的模块在使用APP更新连接参数时基本正常,使用自制的模块更新蓝牙连接参数时出现app  status =0x22 状态,然后蓝牙断开;

请问更新蓝牙连接参数会收硬件的影响吗,具体受哪方面的影响;

测试工具 APP NRF CONNECT 和cc2640r2f ;

连接设置

// it's last parameter set to a static random address
#define DEFAULT_ADDRESS_MODE ADDRMODE_PUBLIC

// General discoverable mode: advertise indefinitely
#define DEFAULT_DISCOVERABLE_MODE GAP_ADTYPE_FLAGS_GENERAL

// Minimum connection interval (units of 1.25ms, 80=100ms) for parameter update request
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 80

// Maximum connection interval (units of 1.25ms, 104=130ms) for parameter update request
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 104

// Slave latency to use for parameter update request
#define DEFAULT_DESIRED_SLAVE_LATENCY 0

// Supervision timeout value (units of 10ms, 300=3s) for parameter update request
#define DEFAULT_DESIRED_CONN_TIMEOUT 300

// Pass parameter updates to the app for it to decide.
#define DEFAULT_PARAM_UPDATE_REQ_DECISION GAP_UPDATE_REQ_PASS_TO_APP

// How often to perform periodic event (in ms)
#define SP_PERIODIC_EVT_PERIOD 300

// How often to read current current RPA (in ms)
#define SP_READ_RPA_EVT_PERIOD 3000

// Delay (in ms) after connection establishment before sending a parameter update requst
#define SP_SEND_PARAM_UPDATE_DELAY 6000