如题:
如何将 一段版本号,写在固定的Flash地址中,并可以生成在Hex文件固定的地址位置? 能否提供参考的示例,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
版本号在devinfoservice.c中写入比较方便,通过Simplelink Starter APP连上CC2642就可以看到设备信息
// Device Information Service attribute
static CONST gattAttrType_t devInfoService = { ATT_BT_UUID_SIZE, devInfoServUUID };
// System ID characteristic
static uint8 devInfoSystemIdProps = GATT_PROP_READ;
static uint8 devInfoSystemId[DEVINFO_SYSTEM_ID_LEN] = {0, 0, 0, 0, 0, 0, 0, 0};
// Model Number String characteristic
static uint8 devInfoModelNumberProps = GATT_PROP_READ;
static uint8 devInfoModelNumber[DEVINFO_STR_ATTR_LEN+1] = "Model Number";
// Serial Number String characteristic
static uint8 devInfoSerialNumberProps = GATT_PROP_READ;
static uint8 devInfoSerialNumber[DEVINFO_STR_ATTR_LEN+1] = "Serial Number";
// Firmware Revision String characteristic
static uint8 devInfoFirmwareRevProps = GATT_PROP_READ;
static uint8 devInfoFirmwareRev[DEVINFO_STR_ATTR_LEN+1] = "Firmware Revision";
// Hardware Revision String characteristic
static uint8 devInfoHardwareRevProps = GATT_PROP_READ;
static uint8 devInfoHardwareRev[DEVINFO_STR_ATTR_LEN+1] = "Hardware Revision";
// Software Revision String characteristic
static uint8 devInfoSoftwareRevProps = GATT_PROP_READ;
static uint8 devInfoSoftwareRev[DEVINFO_STR_ATTR_LEN+1] = "Software Revision";
// Manufacturer Name String characteristic
static uint8 devInfoMfrNameProps = GATT_PROP_READ;
static uint8 devInfoMfrName[DEVINFO_STR_ATTR_LEN+1] = "Manufacturer Name";
在固定地址写入数据可以参考SDK中的例程C:\ti\simplelink_cc13x2_26x2_sdk_5_10_00_48\examples\rtos\CC26X2R1_LAUNCHXL\drivers\nvsinternal