This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: SDK中company id、packet id过滤问题

Part Number: CC2640R2F

您好,

         我们在使用SDK中AOA receiver工程时发现如下问题,希望得到您的帮助。第一个数据包格式可以根据company id,packet id(LocPktTab参数

)过滤,第二种数据包格式则无法过滤获得数据。使用的SDK版本:simplelink_cc2640r2_sdk_2_30_00_28。想了解一下此过滤得机制,如果想要支持第二种数据包格式(比第一种格式PDU部分前面多了三个字节),需要做什么修改,谢谢!

第一种数据包PDU部分

13

adv0

0x1E

adv Len

14

adv1

0xFF

15

adv2

0x0D

TI companyID

16bit

16

adv3

0x00

17

adv4

0x04

AoA packetID

8bit

18

adv5

0x00

padding

6 bytes

19

adv6

0x00

20

adv7

0x00

21

adv8

0x00

22

adv9

0x00

23

adv10

0x00

24

adv11

0xFF

DF signals

20 bytes

25

adv12

0xFF

begin at (1+4+6)byte

26

adv13

0xFF

27

adv14

0xFF

28

adv15

0xFF

29

adv16

0xFF

30

adv17

0xFF

31

adv18

0xFF

32

adv19

0xFF

33

adv20

0xFF

34

adv21

0xFF

35

adv22

0xFF

36

adv23

0xFF

37

adv24

0xFF

38

adv25

0xFF

39

adv26

0xFF

40

adv27

0xFF

41

adv28

0xFF

42

adv29

0xFF

43

adv30

0xFF

第二种PDU部分:

13

adv0

0x02

AD data length

14

adv1

0x01

AD type:Flags

15

Adv2

0x06

Flags Data

16

Adv3

0x1B

AD data length

17

Adv4

0xFF

AD type

18

Adv5

0x0D

TI companyID

16bit

19

Adv6

0x00

20

Adv7

0x04

AoA packetID

8bit

21

Adv8

0x00

22

adv9

0x00

23

adv10

0x00

24

adv11

0xFF

DF signals

20 bytes

25

adv12

0xFF

begin at (1+4+6)byte

26

adv13

0xFF

27

adv14

0xFF

28

adv15

0xFF

29

adv16

0xFF

30

adv17

0xFF

31

adv18

0xFF

32

adv19

0xFF

33

adv20

0xFF

34

adv21

0xFF

35

adv22

0xFF

36

adv23

0xFF

37

adv24

0xFF

38

adv25

0xFF

39

adv26

0xFF

40

adv27

0xFF

41

adv28

0xFF

42

adv29

0xFF

43

adv30

0xFF