This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: CC2652R: simple_peripheral例程和simple_central例程,NV Flash是仅提供给BLE Stack5使用的?

Part Number: CC2652R

如题,仅限于例程。NV Flash芯片是蓝牙协议栈的那个核使用吗?

  • NVS是用于向flash读取和写入数据的驱动程序,所有和应用相关的都是使用的Cortex-M4F,只有射频部分用了Cortex-M0

  • 请问,

    1. 自动连接(auto connect)的思路,就是simple_peripheral和simple_central例程中的靠判断广播数据来匹配的吗?

    2. CC26X2评估板的那个例程,演示了Bond?

    绑定后,如何实现auto connect,还是采用1种的方法吗?

  • 这是另一个问题了,有新问题请开一个一个新帖,方便其他人查找

x 出现错误。请重试或与管理员联系。