第一次使用CC2541,在官网上下载了例程,但是没找到有关于使用外部32.768晶振的例程,请问有这样的例程吗?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您指的是时钟初始化的部分?那您可以看一下 Init_sys_Clock 函数
可以进行如下设置
/******************************************************************************
* @fn Init_Sys_Clock
*
* @brief Crystal selection
* OSC32K register(attention)
* 32-kHz clock-source select. Setting this bit initiates a clock-source change only.
* CLKCONSTA.OSC32K reflects the current setting. The 16-MHz RCOSC must be
* selected as system clock when this bit is to be changed. This bit does not give an
* indication of the stability of the 32-kHz XOSC.
*
* @param cs.high_clock_ex = 1 use external 32MHz clock
* 0 use internal 16MHz clock
* cs.low_clock_ex = 1 use external 32kHz clock
* 0 use internal 32kHz clock
*
* @return NULL
*
******************************************************************************/
void Init_sys_Clock (CLOCK_SOURCE cs )
{
//RC 16MHz
CLKCONCMD = (CLKCONCMD & 0x80) | 0x49;
while ((CLKCONSTA & ~0x80) != 0x49 );
if(cs.low_clock_ex == 1)
{
//XOSC 32kHz
CLKCONCMD = (CLKCONCMD & ~0x80) ;
while ( (CLKCONSTA & 0x80) != 0 );
}
else
{
//RCOSC 32kHz
CLKCONCMD |= 0x80 ;
while ( (CLKCONSTA & 0x80) == 0 );
}
if(cs.high_clock_ex == 1)
{
//XOSC 32MHz
CLKCONCMD = (CLKCONCMD & 0x80) ;
while ( (CLKCONSTA & ~0x80) != 0 );
}
}
您好,请问这是哪个例程里面的函数?是所有例程都有Init_sys_Clock函数吗?在哪里可以看到呢?谢谢
我只是给出相关的配置需要的代码,在例程内的时钟配置定义在hal_board_cfg.h 您可以查看相关的定义
你好,我下载的例程(SWRC257.ZIP 和SWRC251B.ZIP)中,没有hal_board_cfg.h这个头文件。