This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: CC2640R2F 修改MTU 从机判断修改成功标志

Part Number: CC2640R2F

请问:我的手机APP 是主机。 板子是从机。 主机主动修改MTU为251字节,从机怎么判断修改MTU成功? 

  • 修改成功后会在串口打印MTU size信息

    static uint8_t SimplePeripheral_processGATTMsg(gattMsgEvent_t *pMsg)
    {
      if (pMsg->method == ATT_FLOW_CTRL_VIOLATED_EVENT)
      {
        // ATT request-response or indication-confirmation flow control is
        // violated. All subsequent ATT requests or indications will be dropped.
        // The app is informed in case it wants to drop the connection.
    
        // Display the opcode of the message that caused the violation.
        Display_printf(dispHandle, SP_ROW_STATUS_1, 0, "FC Violated: %d", pMsg->msg.flowCtrlEvt.opcode);
      }
      else if (pMsg->method == ATT_MTU_UPDATED_EVENT)
      {
        // MTU size updated
        Display_printf(dispHandle, SP_ROW_STATUS_1, 0, "MTU Size: %d", pMsg->msg.mtuEvt.MTU);
      }
    
      // Free message payload. Needed only for ATT Protocol messages
      GATT_bm_free(&pMsg->msg, pMsg->method);
    
      // It's safe to free the incoming message
      return (TRUE);
    }

  • 你好,请问这个函数是在主机端还是从机端?  我现在是从机端判断。

  • SimplePeripheral 从机的