This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 蓝牙论坛

Part Number: CC2640R2F


请问: 我按照 :    #define APP_SUGGESTED_PDU_SIZE 251 //default is 27 octets(TX)
                               #define APP_SUGGESTED_TX_TIME 2120 //default is 328us(TX)

                              HCI_LE_WriteSuggestedDefaultDataLenCmd(APP_SUGGESTED_PDU_SIZE, APP_SUGGESTED_TX_TIME);

                              #define MAX_PDU_SIZE 251

            上面代码已经成功设置好CC2640R2F 最大MTU为 251字节。

            我用安卓手机开发APP去设置 从机CC2640R2F   MTU,可以正常按照248个字节进行透传。

            但是在用苹果手机开发APP的时候,苹果手机没有开放修改MTU的接口,应该怎么操作?