This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: CC2642 HID功能,发现与iphone连接后,自动回连时间较长

Part Number: CC2642R


目前测试下来,自动回连时间不固定,在2~15s左右,但是把模块重启,就能实现瞬间重连。

请问在断开连接的时候,能否通过清除什么信息,达到自动重连的速度加快;目前,使用HAL_SYSTEM_RESET()函数,发现使用后就会死机,不能通过软件复位实现。

希望能给一些帮助,不知道是否调整重连时间参数,或者别的什么,能够加快这个速度。

另外:HID扫描速度或重连速度与什么有关,与那个参数有关,希望给与帮助,谢谢!

使用hid库:

GitHub - TexasInstruments/HOGP-BLE-HID-EXAMPLE: HOGP (HID Over GATT Profile) BLE Example for the CC26X2 devices.