CCS9.2.0.00013_win64
simplelink_cc13x2_26x2_sdk_3_40_00_02
把simplelink中的simplelink_cc13x2_26x2_sdk_3_40_00_02\examples\rtos\CC26X2R1_LAUNCHXL\ble5stack\rtls_master 导入CCS出现以下报错
[ERROR] IcePick_C: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.4.0.00129)