Part Number: CC2640R2F
Other Parts Discussed in Thread: ADS1291,
在设计AD采集时,会采集到的与蓝牙最小连接间隔相同频率的噪声如何滤除?
如设置最小连接间隔为45ms,采集到的信号会有个22Hz的噪声。
推测蓝牙在发送是会有个22Hz的6ma的大电流,对采集电路产生影响。请问这个噪声如何滤除?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.这个链接间隔是怎么选的?看资料说是从机设定的,是15和45两个时间是二选一吗?还是15-45之间?
2.如果我以比链接时间间隔小的时间发送数据,协议栈会怎么操作,会不会丢失数据?
必须在ble core spec规定的范围内使用
我是用ads1291采集的,此时这个频率干扰幅值比较小,但是也能明显看出。我如果再ads1291前面加个放大器,就会比较大。就像上图中的。
这可能与ads1291和前面的电路有关,你使用CC2640r2f自带的adc接到3.3V或者使用信号发生器给个信号看下是否还会出现类似的
噪声