Other Parts Discussed in Thread: SYSCONFIG
rtls_master和rtls_slave在无连接的状态下获取I/Q数据,是不是rtls_master先扫描,扫描到rtls_slave之后,rtls_slave就会按照一定的时间间隔发送I/Q数据到rtls_master?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
修改周期性广播间隔:
// Periodic Advertising Intervals #define PERIODIC_ADV_INTERVAL_MIN 400 // 500 ms #define PERIODIC_ADV_INTERVAL_MAX 400 // 500 ms // Set Periodic Advertising parameters GapAdv_periodicAdvParams_t perParams = {PERIODIC_ADV_INTERVAL_MIN, PERIODIC_ADV_INTERVAL_MAX, 0x40}; status = GapAdv_SetPeriodicAdvParams(advHandleNCNS, &perParams);
CTE里面是连续的1
在simple_peripheral这个工程里面可以在simple_peripheral.syscfg里面修改,但是在rtls_slave里面就找不到修改广播间隔的地方?
还有就是配置工具里面simple_peripheral选的是BLE,rtls_slave工程选的是Custom,BLE和Custom是什么区别呢?
slave程序不能通过sysconfig广播间隔,slave例程主要基于AOA功能,未在sysconfig文件中添加相关的配置
customer就是可以自己配置的,未在其中添加特定的功能
CTE里面是连续的1,是固定的吗?长度也固定吗?