This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: CCS中无法使用全局静态变量?

Part Number: CC2640R2F

比如 定义static bool ImageCalibrated = false;

、、、

if(ImageCalibrated  == false){

   ImageCalibrated   = true;

   do something;

}

、、、

很简单的依据,但是根部不会执行花括号内的程序,如果把定义变量的static去掉,就能正常执行了。

这是CCS自身的问题还是编译器版本的问题?我用的版本如下:

  • 变量和调用是否在同一文件中,和编译器和CCS都没关系,你可以看到在例程pininterrupt中调用没有问题

    /*
     *  ======== pinInterrupt.c ========
     */
    #include <unistd.h>
    
    /* Driver Header files */
    #include <ti/drivers/PIN.h>
    
    /* Example/Board Header files */
    #include "Board.h"
    
    /* Pin driver handles */
    static PIN_Handle buttonPinHandle;
    static PIN_Handle ledPinHandle;
    
    /* Global memory storage for a PIN_Config table */
    static PIN_State buttonPinState;
    static PIN_State ledPinState;
    
    /*
     * Initial LED pin configuration table
     *   - LEDs Board_PIN_LED0 is on.
     *   - LEDs Board_PIN_LED1 is off.
     */
    PIN_Config ledPinTable[] = {
        Board_PIN_LED0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MAX,
        Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW  | PIN_PUSHPULL | PIN_DRVSTR_MAX,
        PIN_TERMINATE
    };
    
    /*
     * Application button pin configuration table:
     *   - Buttons interrupts are configured to trigger on falling edge.
     */
    PIN_Config buttonPinTable[] = {
        Board_PIN_BUTTON0  | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE,
        Board_PIN_BUTTON1  | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE,
        PIN_TERMINATE
    };
    
    /*
     *  ======== buttonCallbackFxn ========
     *  Pin interrupt Callback function board buttons configured in the pinTable.
     *  If Board_PIN_LED3 and Board_PIN_LED4 are defined, then we'll add them to the PIN
     *  callback function.
     */
    void buttonCallbackFxn(PIN_Handle handle, PIN_Id pinId) {
        uint32_t currVal = 0;
    
        /* Debounce logic, only toggle if the button is still pushed (low) */
        CPUdelay(8000*50);
        if (!PIN_getInputValue(pinId)) {
            /* Toggle LED based on the button pressed */
            switch (pinId) {
                case Board_PIN_BUTTON0:
                    currVal =  PIN_getOutputValue(Board_PIN_LED0);
                    PIN_setOutputValue(ledPinHandle, Board_PIN_LED0, !currVal);
                    break;
    
                case Board_PIN_BUTTON1:
                    currVal =  PIN_getOutputValue(Board_PIN_LED1);
                    PIN_setOutputValue(ledPinHandle, Board_PIN_LED1, !currVal);
                    break;
    
                default:
                    /* Do nothing */
                    break;
            }
        }
    }
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
    
        /* Open LED pins */
        ledPinHandle = PIN_open(&ledPinState, ledPinTable);
        if(!ledPinHandle) {
            /* Error initializing board LED pins */
            while(1);
        }
    
        buttonPinHandle = PIN_open(&buttonPinState, buttonPinTable);
        if(!buttonPinHandle) {
            /* Error initializing button pins */
            while(1);
        }
    
        /* Setup callback for button pins */
        if (PIN_registerIntCb(buttonPinHandle, &buttonCallbackFxn) != 0) {
            /* Error registering button callback function */
            while(1);
        }
    
        /* Loop forever */
        while(1) {
            sleep(1000);
        }
    }
    

  • 就是在同一文件,测试了很多次,都是这样

  • 我试了没有问题,你用上面的例程试一下