Part Number: CC2642R
关于CC2642将LNA/PA映射到IO上的相关问题
1、我通过【
IOCPortConfigureSet(IOID_6, IOC_PORT_RFC_GPO0,IOC_IOMODE_NORMAL); IOCPortConfigureSet(IOID_7, IOC_PORT_RFC_GPO3,IOC_IOMODE_NORMAL);】方法将LNA以及TX相关映射到MCU的IO上,此时该设备作为主机(central)。并连接一个从机,进行蓝牙通信
2、此时我用示波器可以在对应的IO上可以看到蓝牙通信的连接间隔,如下图所示,其中峰值代表的是主从机进行数据通信的时刻

3、我想进行以下操作:因为每个峰值代表一个连接事件,我想使用类似上升沿/下降沿中断的方式,每一个峰值到来时触发中断。但是因为这个IO已经被重映射了,所以原本的IO功能已经丧失,请问将LNA/PA映射到IO上之后当连接事件到来时(峰值)怎么触发中断??
4、我查阅手册,如下图所示,将LNA/PA映射到IO上之后,要想使能的话需要将对应电平设置为高电平,此时IO管脚的功能已经被覆盖,该怎么把管脚电平拉高呢?