我想用CC2640R2F的蓝牙与笔记本蓝牙4.0进行通信,电脑搜索不到。是该芯片内部的BLE与4.0不兼容吗?请问有没有相关的解决办法,非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最简单的办法就是打开电脑蓝牙看能不能搜到BLE的广播
查看PC蓝牙的型号,看是否支持BLE,不过一般的蓝牙4.0的设备应该是不支持BLE的
我查了我的电脑蓝牙是5.0,能够搜索到,但是连接不上。是不是用的SDK不对?还是修改一下就行?非常感谢!
用例程simple_peripheral应该可以连接上,将BLE设备直接与电脑连接似乎作用不大,因为PC无法直接对它进行操作
通常需要额外的BLE设备通过UART与电脑连接,实现其他功能
好的,感谢!我是打算通过电脑蓝牙连接成功后,开发对应的上位机进行操作。