This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 烧录程序成功但是无广播信号且仿真报错

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC3200

使用XDS110烧录器,Flash Programmer 2烧录hex程序,识别芯片没问题,烧录也显示成功了,但是搜索不到蓝牙信号,都是自己做的板子,有的有信号,有的没信号。使用code composer studio进行仿真时,出现以下报错。

Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.2.0.00002)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.2.0.00002)

有广播的板子是没有报错的,只有搜索不到广播的板子仿真会报错。

不知道是哪里出了问题,外围电路的电压也测了是正常的。

  • 出现这两个错误通常是硬件有问题,检查硬件设计,尤其是电源部分和高频晶振部分

    结合上面的部分设备没有广播,你要重点检查外部高频是否起振,以及频率是否准确

    以下是关于两个错误的详细说明:

    This error is caused by the inability of the JTAG debugger to access the DAP or one of its ARM subcores. This is usually caused by either a hardware failure on the board or invalid code on the subcore that causes it to reset itself continuously.

    If this error is originated in software, it can potentially be recovered by accessing the DAP directly and trying to either reset the offending core, lock it or erase its flash memory via a GEL script (some microcontrollers have pre-loaded routines to allow that).

    Notes:

    • Some users reported this error also happens in conjunction with the Invalid device ID error above.
    • For certain devices such as CC13xx and CC26xx, the GEL script is directly available on the menu Scripts → <device name> → MassErase.
    • A procedure to try and unlock a Hercules device is described in this e2e forum thread.
    • For CC3200/CC3220 devices, a few issues can cause this:
      • If using a Launchpad, the SOP jumpers may be set to "Flash" and not JTAG or SWD. Check this e2e thread for a more thorough procedure.
      • The device may also be in production mode. Check this e2e thread for details.
      • The device may be locked due to firmware problems, either the Service Pack or the Application firmware. Check the Launchpad and SDK documentation for details.
    • For C6000 and SoC devices (Sitara, Keystone 2, etc.), check item 8 of the section Troubleshooting the connect phase above.
    • For all Launchpad boards that use the XDS110 Debug Probe, a recent change on the default TCLK speed may cause this issue. Please check the section JTAG clock speed considerations at the XDS110 page.


        Error: (Error -1170 @ 0x0)
        Unable to access the DAP. Reset the device, and retry the operation.
        If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). 
        

    This error is caused by the inability of the debug probe to communicate with the device.

    This can be caused by a number of hardware problems such as improper reset or power applied to the device, issues with clock (external crystal or oscillator). In this particular case, it is mandatory to verify all hardware details of your system.

    This can also be caused by faulty software running on the device, which causes the core to be on an unstable state. For flash-based devices, you may need to unlock or mass erase the device. Check step 9 of the section Troubleshooting the connect phase above.

    This error usually happens together with the Cannot Access the DAP error above.

    Trouble Halting Target CPU: (Error -2064 @ 0x0)
    Unable to read device status. Reset the device and try the operation again.
    If the error persists, check the configuration, power cycle the board,
    and try to make JTAG settings more stable (for example, lower TCLK).

  • 贴片场晶振虚焊了。。是外围高速晶振的问题。感谢