This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2640R2F
是可以调整内部匹配电容吗?
内部电容匹配阵列是用来调整高频crystal的,可以广播而不能连接大概率是32K低频晶振的问题
检查低频晶振是否存在频率偏移,焊接是否正确
可以将新信号映射到IO上测量频率是否准确,添加以下代码:
#include <driverlib/aon_ioc.h>IOCPortConfigureSet(IOIDn, IOC_PORT_AON_CLK32K, IOC_STD_OUTPUT);AONIOC32kHzOutputEnable();
32.768kHz晶振的频率信号,使用您的代码,会输出在哪个管脚上?
修改IOIDn指定IO引脚,可以将其设置为认为我未使用的GPIO
例如:IOID_0代表DIO0
测得结果为32.58kHz,是否正常呢?
不正常,根据bluetooth core spec规范,从机时钟至少需要 ±500ppm 的精度
你需要调低频晶振的负载电容保证低频时钟准确,建议遵循参考设计文件