This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 如何使用RTC实现毫秒级周期性唤醒

Part Number: CC2640R2F


目前手头上有一低功耗项目大概要求:MCU在空闲时进入standby睡眠,10ms左右唤醒一次MCU,执行一次I/O电平操作,执行完再睡眠10ms,再执行一次I/O电平操作.....

请问,

1.CC2640R2F在standby模式下,能否使用RTC通道2的连续比较模式来进行周期性唤醒呢?要求是毫秒级的周期性唤醒

2.如果1可以实现,那么SDK中有没有相关例程可供参考??

3.如果1可以实现,那么从RTC通道2唤醒事件发生,经过Power domain重新初始化,再到执行完成I/O电平操作,整个唤醒流程大概需要多久?

谢谢