Part Number: CC2640R2F
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
选择此项时,一切正常。
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
选择此项,只能广播,连接总是失败。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
实际情况让人很无语:
1、
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
选择此项时,一切正常。
//#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
测量31.25kHz
选择此项时,一切正常。
2、
//#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
测量31.55kHz
只能广播,连接总是失败。
3、
//#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC
将8pF电容更换原有7pF电容
测量32.77kHz
一切正常。