求一个适用于cc2640r2f的4*4封装的高速串口透传例程,需要传输速率能达到10kb/s,主要是能处理每2ms发送8个字节(1秒大约4118个字节)的数据包然后不丢包的全部发送出来,谢谢大家
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求一个适用于cc2640r2f的4*4封装的高速串口透传例程,需要传输速率能达到10kb/s,主要是能处理每2ms发送8个字节(1秒大约4118个字节)的数据包然后不丢包的全部发送出来,谢谢大家
ble min connection interval一般是7.5ms,你要每2ms发送一个数据包基本上是做不到
您好,那请问有没有其他方法能把以8个字节的数据包以2ms发送一次(大约4200的字节)的数据不丢包的发送给出来呢,比如先放入缓冲区再集中发送出来
如果ble min connection interval設置是7.5ms,最短的发送间隔基本上就是不能低於7.5 ms
試試用 https://github.com/ti-simplelink/ble_examples/tree/simplelink_sdk-1.35/examples/rtos/CC2640R2_LAUNCHXL/ble5apps 的例程去調整connection interval看看能否符合你的需求