static void RssiRead( int8 newRSSI )
这个newRSSI 值,怎么换成DB,,应该是负数到0吧。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
static void RssiRead( int8 newRSSI )
这个newRSSI 值,怎么换成DB,,应该是负数到0吧。
RSSI value (-127..20dBm), or not available
CC2540DK的做法如下。另外你也可以看看,rssi类型是int8即signed char范围是-128~127,最高位是符号位。
static void simpleBLECentralRssiCB( uint16 connHandle, int8 rssi )
{
LCD_WRITE_STRING_VALUE( "RSSI -dB:", (uint8) (-rssi), 10, HAL_LCD_LINE_1 );
}
我理解是-59好。当然,简单的一个测试就行,你拉近拉远,然后看看是怎么变化的不就清楚了。
按这个方法
GAPRole_SetParameter(GAPROLE_RSSI_READ_RATE,sizeof(uint16),&desired_rssi_rate);
这个是设置RSSI的读取速率,默认是0,所以你要设一个非零值,然后如下,就不详细列了,你跟一下GAPROLE_RSSI_READ_RATE应该差不多就明白了。
static void RssiRead( int8 newRSSI ); static void RssiRead( int8 newRSSI ) { //你的处理 }
// GAP Role Callbacks static gapRolesCBs_t keyFob_PeripheralCBs = { peripheralStateNotificationCB, // Profile State Change Callbacks RssiRead // When a valid RSSI is read from controller };
然后static void RssiRead( int8 newRSSI ) 这个newRSSI,的值,在旁边时202,远点195 换成无符号应该是-75 -59。