hi,
我在simplebleperipheral 里的 simpleProfileChangeCB函数里,
用代码 P1_6=1 控制该口输出低电平, P1_6=0 输出高电平
测试发现两种情况都是低电平,去掉POWER_SAVING试验还是一样
使用P1_1=1控制LED灯,就没有问题,是哪里上拉下拉电阻没设对么 怎么设
请问哪里出问题了,先谢谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yan ,
我使用TI的例程simpleBLEPeripheral,配置方面没有修改,仅仅在simpleProfileChangeCB中添加了IO口控制代码,例程中的IO口配置如下:
P0SEL = 0; // Configure Port 0 as GPIO
P1SEL = 0; // Configure Port 1 as GPIO
P2SEL = 0; // Configure Port 2 as GPIO
P0DIR = 0xFC; // Port 0 pins P0.0 and P0.1 as input (buttons),
// all others (P0.2-P0.7) as output
P1DIR = 0xFF; // All port 1 pins (P1.0-P1.7) as output
P2DIR = 0x1F; // All port 1 pins (P2.0-P2.4) as output
P0 = 0x03; // All pins on port 0 to low except for P0.0 and P0.1 (buttons)
P1 = 0; // All pins on port 1 to low
P2 = 0; // All pins on port 2 to low