This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: 如何在CC2652R上使用2Mbps+调制速率的HS mode高速模式

Part Number: CC2652R
Other Parts Discussed in Thread: CC1310

我们项目需要2Mbps左右的无线传输速率,ti cc2652 SDK里面提供的RF相关例程似乎没有能达到2Mbps+的传输速率。此外,我在cc2652R的技术参考手册中看到CMD_RADIO_SETUP命令可以设置radio的模式,附图如下

请问如何使用2-Mbps GFSK或者5-Mbps coded 8-FSK模式进行数据传输?不限于在CC2652R上实现,其他型号的也可以。

感谢!

  • 请问如何使用2-Mbps GFSK或者5-Mbps coded 8-FSK模式进行数据传输?不限于在CC2652R上实现,其他型号的也可以。

    支持这种模式,但没有为此提供程序

    CC1310、CC2640r2上有一个HS Mode示例可以达到4 MBit/s的速率:

    C:\ti\simplelink_cc2640r2_sdk_5_30_00_03\examples\rtos\CC2640R2_LAUNCHXL\drivers\rfPacketErrorRate

  • 感谢Kevin!如果我想通过CMD_RADIO_SETUP更改mode并在cc2652R上构造程序实现数据高速传输,此方案是否具有可行性?

    我们想实现2Mbps左右的实际传输速率,不知道能否请求你的建议,比如选择哪种型号的simplelink芯片更好?从哪个例程入手更容易实现?

    谢谢Kevin!

    支持这种模式,但没有为此提供程序

  • 如果我想通过CMD_RADIO_SETUP更改mode并在cc2652R上构造程序实现数据高速传输,此方案是否具有可行性?

    可行,但是没有提供指导文档和相关的驱动程序,实现起来可能有些难度

    我们想实现2Mbps左右的实际传输速率,不知道能否请求你的建议,比如选择哪种型号的simplelink芯片更好?从哪个例程入手更容易实现?

    可以使用CC1310,参考例程:

    C:\ti\simplelink_cc13x0_sdk_4_20_01_03\examples\rtos\CC1310_LAUNCHXL\drivers\rfPacketErrorRate

  • 谢谢Kevin!已经解答了我的问题 : )