Part Number: CC2640
简单外设 例程 如果更改外设名称?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在simple_peripheral.c中找到下面代码进行修改:
// Scan Response Data
static uint8_t scanRspData[] =
{
// complete name
17, // length of this data
GAP_ADTYPE_LOCAL_NAME_COMPLETE,
'S',
'i',
'm',
'p',
'l',
'e',
'P',
'e',
'r',
'i',
'p',
'h',
'e',
'r',
'a',
'l',
// connection interval range
5, // length of this data
GAP_ADTYPE_SLAVE_CONN_INTERVAL_RANGE,
LO_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL), // 100ms
HI_UINT16(DEFAULT_DESIRED_MIN_CONN_INTERVAL),
LO_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL), // 1s
HI_UINT16(DEFAULT_DESIRED_MAX_CONN_INTERVAL),
// Tx power level
2, // length of this data
GAP_ADTYPE_POWER_LEVEL,
0 // 0dBm
};