This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: I2C 问题

Part Number: CC2642R
Other Parts Discussed in Thread: SYSBIOS

我需要动态的开关I2C Slave 模式(为了省电)

int8_t hpi_i2c_open()
{
    if(m_is_open == 0)
    {
        Power_setDependency(PowerCC26XX_PERIPH_I2C0);
        Power_setConstraint(PowerCC26XX_SB_DISALLOW);
        Power_setConstraint(PowerCC26XX_IDLE_PD_DISALLOW);
        i2cPinHandle = PIN_open(&i2cPinState, i2cPinTable);
        if ((PIN_SUCCESS == PINCC26XX_setMux(i2cPinHandle, CONFIG_PIN_2,    IOC_PORT_MCU_I2C_MSSCL))
                && (PIN_SUCCESS == PINCC26XX_setMux(i2cPinHandle, CONFIG_PIN_1,IOC_PORT_MCU_I2C_MSSDA))) {
            LOGI("I2C PIN set succ.");
        } else {
            LOGI("I2C PIN set failed.");
        }
        /* init i2c for slave-mode and enable interrupt */
        I2CSlaveInit(I2C0_BASE, slaveAddress);
        LOGI("I2CSlaveInit.");
        /* Create an RTOS aware hardware interrupt */
        Hwi_Params i2cSlave_hwiParams;
        Hwi_Params_init(&i2cSlave_hwiParams);
        LOGI("Hwi_Params_init.");
        i2cSlave_hwiParams.priority = INT_PRI_LEVEL7; //INTERRUPT_PRIORITY;
        i2cSlave_hwiHandle = Hwi_create(INT_I2C_IRQ, i2cCB, &i2cSlave_hwiParams,NULL);
        LOGI("Hwi_create.");
        if (NULL == i2cSlave_hwiHandle) {
            //some error occurred
            LOGI("i2c init error");
            return -1;
        }
        I2CSlaveIntEnable(I2C0_BASE,
        I2C_SLAVE_INT_START | I2C_SLAVE_INT_STOP | I2C_SLAVE_INT_DATA);
        m_is_open = 1;
        LOGW("i2c open ok!!");
    }

    return 0;
}
int8_t hpi_i2c_close()
{
    if(m_is_open == 1)
    {
        PIN_close(i2cPinHandle);
        Hwi_delete(i2cSlave_hwiHandle);
        Power_releaseDependency(PowerCC26XX_PERIPH_I2C0);
        Power_releaseConstraint(PowerCC26XX_SB_DISALLOW);
        Power_releaseConstraint(PowerCC26XX_IDLE_PD_DISALLOW);
        m_is_open = 0;
        LOGW("i2c close ok!!");
    }
    return 0;
}
代码如上。
进行open ->close ->open 时 卡在Hwi_create里面。请问怎样解决。