This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: scifWaitOnNbl的使用問題

Part Number: LAUNCHXL-CC1352R1


  * \b Important: Unlike the ALERT event, the READY event does not generate MCU domain and System CPU
  * wake-up. Depending on the SCIF OSAL implementation, this function might not return before the
  * specified timeout expires, even if the READY event has occurred long before that. To avoid such
  * delays, call \c fwGenAlertInterrupt() from the task code block that \ref scifWaitOnNbl() is waiting
  * for to complete.

請問" call \c fwGenAlertInterrupt() from the task code block that \ref scifWaitOnNbl() is waiting for to complete." 此句的用意是?

看起來是要在sensor controller studio中, 加入fwGenAlertInterrupt() .

但是要怎麼跟scifWaitOnNbl() is waiting for to complete有相關聯呢?

  • 您好我们已收到您的问题并升级到英文论坛寻求帮助,链接如下,如有答复将尽快回复您。谢谢!

    e2e.ti.com/.../launchxl-cc1352r1-scifwaitonnbl

  • Hi,

    方便补充一下上下文吗?您是在哪个project中找到这一部分的?

  • 此段是出現在scif_framework.c中的 scifWaitOnNbl function

    在multi_sensor_CC1352R1_LAUNCHXL_tirtos_ccs可以找到

    Drivers->ACCELEROMETER->scif_framework.c

    /** \brief Waits for a non-blocking call to complete, with timeout
      *
      * The non-blocking task control functions, \ref scifExecuteTasksOnceNbl(), \ref scifStartTasksNbl()
      * and \ref scifStopTasksNbl(), may take some time to complete. This wait function can be used to make
      * blocking calls, and allow an operating system to switch context when until the task control interface
      * becomes ready again.
      *
      * The function returns when the last non-blocking call has completed, or immediately if already
      * completed. The function can also return immediately with the \ref SCIF_ILLEGAL_OPERATION error if
      * called from multiple threads of execution with non-zero \a timeoutUs.
      *
      * \b Important: Unlike the ALERT event, the READY event does not generate MCU domain and System CPU
      * wake-up. Depending on the SCIF OSAL implementation, this function might not return before the
      * specified timeout expires, even if the READY event has occurred long before that. To avoid such
      * delays, call \c fwGenAlertInterrupt() from the task code block that \ref scifWaitOnNbl() is waiting
      * for to complete.
      *
      * \param[in]      timeoutUs
      *     Maximum number of microseconds to wait for the non-blocking functions to become available. Use a
      *     timeout of "0" to check whether the interface already is available, or simply call the control
      *     function (which also will return \ref SCIF_NOT_READY if not ready).
      *
      * \return
      *     \ref SCIF_SUCCESS if the last call has completed, otherwise \ref SCIF_NOT_READY (the timeout
      *     expired) or \ref SCIF_ILLEGAL_OPERATION (the OSAL does not allow this function to be called with
      *     non-zero \a timeoutUs from multiple threads of execution).
      */
    SCIF_RESULT_T scifWaitOnNbl(uint32_t timeoutUs) {
        if (HWREG(AUX_EVCTL_BASE + AUX_EVCTL_O_EVTOAONFLAGS) & AUX_EVCTL_EVTOAONFLAGS_SWEV0_M) {
            return SCIF_SUCCESS;
        } else {
            return osalWaitOnCtrlReady(timeoutUs);
        }
    } // scifWaitOnNbl

  • 好的我们跟进给工程师看下。

  • 您好,

    任务控制函数 scifExecuteTasksOnceNbl()不会阻止执行并立即返回。 但一次性只能调用这些函数一次:

    例如,不能连续两次调用 scifExecuteTasksOnceNbl(),而不在两次调用之间等待。 在这两个呼叫之间等待 scifWaitOnNbl (timeout)。

    当 CPU 等待 scifWaitOnNbl()时,可能进入睡眠状态。 如果sensor controller仅发布一个READY event并且需要一个ALERT event来唤醒,那么CPU 不会被唤醒。

    如果 scifExecuteTasksOnceNbl()所调用任务的sensor controller代码中没有 fwGenAlertInterrupt(),则该任务仅生成READY event,因此 CPU 仅在timeout时唤醒。 但是该任务可能在这个timeout之前就已经完成执行。

    如果您希望sensor controller上的任务完成后 CPU 立即唤醒,则可以让 fwGenAlertInterrupt()生成ALERT event。 这将唤醒 CPU。