Part Number: CC2640R2L
我需要实现使用两个定时器进行广播切换的功能,在定时器A的事件触发时进行自定义广播包的切换,在定时器B事件触发时,进行标准广播包的切换,并循环持续30s,但是当第一个广播包切换后,定时出现异常,且其他的触发事件都出现了异常,例如串口,按键,都无法触发了,请问这是什么情况导致的。
我的代码如下:
#define SP_ADV_SOS_EVT_PERIOD 300
advInt = 160
Util_constructClock(&advsos, SimplePeripheral_clockHandler,
SP_ADV_SOS_EVT_PERIOD, 0, false, (UArg)&argadvsos);
Util_constructClock(&advupade, SimplePeripheral_clockHandler,
advInt * 0.625, 0, false, (UArg)&argadvupade);
static void adv_init()
{
//Method 1
if (sos_state == 1)
memcpy(updateAdvData, advertDataNew, sizeof(advertDataNew));
else if(sos_state == 0)
memcpy(updateAdvData, advertData, sizeof(advertData));
bStatus_t status = FAILURE;
status = GapAdv_prepareLoadByHandle(advHandleLegacy,GAP_ADV_FREE_OPTION_ADV_DATA);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
// Load advertising data for set #1 that is statically allocated by the app
status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV,
sizeof(updateAdvData), updateAdvData);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
//Method 2
/*
GapAdv_params_t advParamLegacy;
advParamLegacy.eventProps = GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_SCANNABLE | GAP_ADV_PROP_LEGACY;
advParamLegacy.primIntMin = advInt;
advParamLegacy.primIntMax = advInt;
advParamLegacy.primChanMap = GAP_ADV_CHAN_ALL;
advParamLegacy.peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID;
//memcpy(advParamLegacy.peerAddr, pPkt->devAddr, B_ADDR_LEN);
advParamLegacy.filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ;
advParamLegacy.primPhy = GAP_ADV_PRIM_PHY_1_MBPS;
advParamLegacy.secPhy = GAP_ADV_SEC_PHY_1_MBPS;
advParamLegacy.sid = 0;
// Create Advertisement set #1 and assign handle
status = GapAdv_create(&SimplePeripheral_advCallback, &advParamLegacy,
&advHandleLegacy);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
// Load advertising data for set #1 that is statically allocated by the app
status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_ADV,
sizeof(updateAdvData), updateAdvData);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
// Load scan response data for set #1 that is statically allocated by the app
status = GapAdv_loadByHandle(advHandleLegacy, GAP_ADV_DATA_TYPE_SCAN_RSP,
sizeof(scanRspData), scanRspData);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
// Set event mask for set #1
status = GapAdv_setEventMask(advHandleLegacy,
GAP_ADV_EVT_MASK_START_AFTER_ENABLE |
GAP_ADV_EVT_MASK_END_AFTER_DISABLE |
GAP_ADV_EVT_MASK_SET_TERMINATED);
// Enable legacy advertising for set #1
status = GapAdv_enable(advHandleLegacy, GAP_ADV_ENABLE_OPTIONS_USE_MAX, 0);
SIMPLEPERIPHERAL_ASSERT(status == SUCCESS);
*/
}
static void SimplePeripheral_processAppMsg(spEvt_t *pMsg)
{
bool dealloc = TRUE;
switch (pMsg->event)
{
...
case SP_ADV_SOS_EVT:
sos_start_handler();
break;
case SP_ADV_UPDATE_EVT:
adv_start_handler();
break;
default:
// Do nothing.
break;
}
}
static void sos_start_handler(void)
{
flag_status.adv_clock_ticks++;
Util_startClock(&advsos);
if (flag_status.adv_clock_ticks == 50)
{
Uart0_Write("Stop\r\n", 6);
flag_status.adv_clock_ticks = 0;
GapAdv_disable(advHandleLegacy);
sos_state = 0;
adv_init();
Util_stopClock(&advsos);
Util_stopClock(&advupade);
}
else
{
Uart0_Write("sos\r\n", 5);
sos_state = 1;
adv_init();
}
}
static void adv_start_handler(void)
{
Uart0_Write("adv\r\n", 5);
Util_startClock(&advupade);
sos_state = 0;
adv_init();
}
如果我把代码中的adv_init()屏蔽以后,在定时器事件中添加串口log,发现定时器可以进行触发,其他事件也可以正常进行。
该方法更新数据是可以正常工作的: