This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: CC2642R1F能利用RSSI信号来做定位吗?

Part Number: CC2642R

您好!请教一个问题:

   我在网上看到一段话:

”蓝牙5.0由于发射功率较大,是4.2的4倍功率,功率大也即发射距离长,但是信号衰减与距离的变化相关性不大,所以无法通过RSSI来进行定位。准确的讲,蓝牙5.0不适合信号发射端,也即不适合作为蓝牙信标使用,但是可以作为蓝牙的接收端,也即蓝牙终端,如手环、胸牌。

蓝牙联盟在蓝牙5.1中加入到到达角度定位,也即蓝牙AoA,这和蓝牙5.0在定位上有本质的区别“

那么,CC2642R是BLE5.2,用户能利用CC2642R的RSSI信号来做定位吗?

我们的产品,CC2642R是主机。和别的公司合作开发。现在对方定位不准,老说是因为我们的板子rssi信号不稳定造成的...。

设备放着不动rssi都有波动,何况他们是利用人行走时身上携带的这个2642设备发出的RSSI来进行定位测距。(如果加上算法及信号传播,处理等时差,如果有个2~3秒,人都已经走了好几米了吧?)感觉是不是大的方案(利用CC2642R的RSSI来测距)有问题啊?