This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 请问CC2640R2F吞吐率提升的思路?

Part Number: CC2640R2F


基本情况是这样的:自己做的板子,SDK版本4.2,协议栈版本5.0,基于SIMPLE PERIPHERAL例程写的程序,通过Character5进行数据传输。

参考相关资料进行了以下的设置:

#define APP_SUGGESTED_PDU_SIZE 251 //default is 27 octets(TX)
#define APP_SUGGESTED_TX_TIME 2120

HCI_LE_WriteSuggestedDefaultDataLenCmd(APP_SUGGESTED_PDU_SIZE, APP_SUGGESTED_TX_TIME);

#define MAX_NUM_PDU                   6

#define MAX_PDU_SIZE                  251

物理层速率1M,TX POWER= 0dbm.就在板子旁边(RSSI -40多)使用手机上的蓝牙调试助手用1个20多K大小的文件进行传输测试,MTU更新为251.

连接间隔最小设置为100毫秒,最大1秒。

但是测量结果显示速率只有502B/s.请问有可能是哪里的问题使得吞吐率这么低?