This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: RSSI

Part Number: CC2640R2F


尊敬的TI工程师你好!

       使用两块LAUNCH PAD  连接到smartrf studio测量RSSI , 发送功率为5dB,每次发送100个包,将一块LAUNCH PAD固定不动,移动另外一块LAUNCH PAD(只平移,高低不变),在记录RSSI的时候,发现0.5m的RSSI要小于0.7m的RSSI,但是按照理论的话0.5m的RSSI是应该大于0.7m的RSSI,而我的0.5m的RSSI为什么会小于0.7m的RSSI?请问RSSI除了和距离、发射功率有关,还和什么有关系呢?

  • 您好,

    理论上在您使用同样器件测试的情况下RSSI只和距离、发射功率有关。但实际情况下也会受外界环境干扰,例如温度大气压特别还有周围2.4GHz频段干扰等。

    其次,0.5m和0.7m这两点的差距其实并不是很大,也有可能是一定的误差。