case GAPROLE_CONNECTED:
{
linkDBInfo_t linkInfo;
uint8_t numActive = 0;
uint8 MacAddr[8] = {0}; //!< Other Device's address
numActive = linkDB_NumActive();
// Use numActive to determine the connection handle of the last
// connection
if ( linkDB_GetInfo( numActive - 1, &linkInfo ) == SUCCESS )
{
Display_print1("Num Conns: %d\r\n", (uint16_t)numActive );
Display_print1("addr NEW:%s\r\n",Util_convertBdAddr2Str(linkInfo.addr));
linkInfo.addrd地址是随机的,怎样可以获取到主机的静态地址呢?