Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2650
自己参照CC2650的评估板,完成了PCB的打板,将除了射频模块的其余电路焊接完成,但是目前没办法完成代码的烧录。测试电压显示VDDS是3.3,VDDR和DCDC_SW几乎没有电压只有0.3V左右。
当使用CCS进行烧录,出现以下报错:
Error connecting to the target:
(Error -242 @ 0x0)
A router subpath could not be accessed.
The board configuration file is probably incorrect.
(Emulation package 9.9.0.00040)
当使用SmartRF进行烧录,使用的是官方的LAUNCHXL-CC2640R2F板上的XDS110进行烧录,SmartRF出现两个COM
当点开第一个COM(XDS110,XDS-L5。。。)出现报错
点开第二个之后,在左下角选择芯片型号进行烧录,出现以下报错
麻烦各位帮忙看看~ 十分感谢