Part Number: CC2640R2F
Other Parts Discussed in Thread: SIMPLELINK-CC2640R2-SDK, CC2650,
使用EasyLink_getIeeeAddr获取IEEE地址时,返回的值为是0xFFFFFFFFFFFFFFFF,而且多块板子都是这个值,为什么?
难道EasyLink_getIeeeAddr不能获取IEEE地址?
如何解决?望帮助,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2640R2F
Other Parts Discussed in Thread: SIMPLELINK-CC2640R2-SDK, CC2650,
使用EasyLink_getIeeeAddr获取IEEE地址时,返回的值为是0xFFFFFFFFFFFFFFFF,而且多块板子都是这个值,为什么?
难道EasyLink_getIeeeAddr不能获取IEEE地址?
如何解决?望帮助,谢谢!
您使用的是哪个版本的 SIMPLELINK-CC2640R2-SDK? EasyLink 应该使用位于 FCFG1 ROM 存储器中的主要 IEEE 地址(用户不能更改),该地址由 TI 工厂在生产期间配置。这仅适用于您未在 CCFG 内提供辅助 IEEE 地址(通过从该位置读取所有 0xFF 来确定)的情况。您可以一步调试 EasyLink.c 以确定发生了什么故障。
//Primary IEEE address location
#define EASYLINK_PRIMARY_IEEE_ADDR_LOCATION (FCFG1_BASE + FCFG1_O_MAC_15_4_0)
//Secondary IEEE address location
#define EASYLINK_SECONDARY_IEEE_ADDR_LOCATION (CCFG_BASE + CCFG_O_IEEE_MAC_0)
//...
EasyLink_Status EasyLink_getIeeeAddr(uint8_t *ieeeAddr)
{
EasyLink_Status status = EasyLink_Status_Param_Error;
if (ieeeAddr != NULL)
{
int i;
//Reading from primary IEEE location...
uint8_t *location = (uint8_t *)EASYLINK_PRIMARY_IEEE_ADDR_LOCATION;
/*
* ...unless we can find a byte != 0xFF in secondary
*
* Intentionally checking all 8 bytes here instead of len, because we
* are checking validity of the entire IEEE address irrespective of the
* actual number of bytes the caller wants to copy over.
*/
for (i = 0; i < 8; i++) {
if (((uint8_t *)EASYLINK_SECONDARY_IEEE_ADDR_LOCATION)[i] != 0xFF) {
//A byte in the secondary location is not 0xFF. Use the
//secondary
location = (uint8_t *)EASYLINK_SECONDARY_IEEE_ADDR_LOCATION;
break;
}
}
//inverting byte order
for (i = 0; i < 8; i++) {
ieeeAddr[i] = location[8 - 1 - i];
}
status = EasyLink_Status_Success;
}
return status;
}首先谢谢你的回复。
情况如下:
1、simplelink_cc2640r2_sdk_4_20_00_04、simplelink_cc2640r2_sdk_3_20_00_21 都用过,结果都是0xFFFFFFFFFFFFFFFF;
2、你给出的代码是EasyLink.c中的函数部分,这些代码我们单步运行过, ieeeAddr[i]都是0xFF。建议你们帮忙实际测试一下试试看?
此行为是 CC2640R2F 不支持 IEEE MAC/PHY 的结果,因此 IEEE MAC 地址在生产期间未编程到 FCFG,CC2650 等设备会观察到有效地址。您可以使用 BLE MAC 地址在 CC2640R2F 上获得唯一地址,即将 EASYLINK_PRIMARY_IEEE_ADDR_LOCATION 更改为引用 FCFG1_O_MAC_BLE_0 而不是 FCFG1_O_MAC_15_4_0。同样,EASYLINK_SECONDARY_IEEE_ADDR_LOCATION 应改为 CCFG_O_IEEE_BLE_0 而不是 CCFG_O_IEEE_MAC_0。