Other Parts Discussed in Thread: CC2640,
我想请问一下,CC2640或者CC2640R2L 是否有加密连接的功能,如果有,那么该功能是如何实现的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我有两个关于配对的问题想要请教一下
1、我在初始设置时已经把配对后绑定选项设置成false了,但是使用手机成功连接后还是会自动绑定设备。设置的代码如下
// Don't send a pairing request after connecting; the peer device must //uint32_t passkey = 0; // passkey "000000" // initiate pairing uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE; // Use authenticated pairing: require passcode. uint8_t mitm = TRUE; // This device only has display capabilities. Therefore, it will display the // passcode during pairing. However, since the default passcode is being // used, there is no need to display anything. uint8_t ioCap = GAPBOND_IO_CAP_DISPLAY_ONLY; // Request bonding (storing long-term keys for re-encryption upon subsequent // connections without repairing) uint8_t bonding = FALSE; uint8_t gapbondSecure = GAPBOND_SECURE_CONNECTION_NONE;//GAPBOND_SECURE_CONNECTION_ONLY ; GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &gapbondSecure); //GAPBondMgr_SetParameter(GAPBOND_DEFAULT_PASSCODE, sizeof(uint32_t), &passkey); GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode); GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm); GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap); GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);
2、我在启动配置后进入密钥连接事件,按照我的需求是如果连接密钥输入错误会断开连接。但是实际输入错误的密钥后,设备反而会快速连接。我在此处设置的代码是否有问题?
我在配对完成后的事件中添加了断开连接的处理事件。
/********************************************************************* * @fn SimplePeripheral_processPairState * * @brief Process the new paring state. * * @return none */ static void SimplePeripheral_processPairState(spPairStateData_t *pPairData) { uint8_t state = pPairData->state; uint8_t status = pPairData->status; switch (state) { case GAPBOND_PAIRING_STATE_STARTED: Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Pairing started"); break; case GAPBOND_PAIRING_STATE_COMPLETE: if (status == SUCCESS) { Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Pairing success"); } else { //Disconnected HCI_EXT_DisconnectImmedCmd(); Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Pairing fail: %d", status); } break; case GAPBOND_PAIRING_STATE_ENCRYPTED: if (status == SUCCESS) { Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Encryption success"); } else { Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Encryption failed: %d", status); //HCI_EXT_DisconnectImmedCmd(); } break; case GAPBOND_PAIRING_STATE_BOND_SAVED: if (status == SUCCESS) { Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Bond save success"); } else { //Display_printf(dispHandle, SP_ROW_CONNECTION, 0, "Bond save failed: %d", status); //HCI_EXT_DisconnectImmedCmd(); } break; default: break; } }