This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: CCS中Debug->System Reset錯誤

Part Number: LAUNCHXL-CC1352R1

CCS: Version: 12.1.0.00007

硬體無修改(LAUCHXL-CC1352R1, chip rev E), 直接使用example, project Zero SDK:simplelink_cc13xx_cc26xx_sdk_6_30_00_84

當使用Debug->System Reset時 就會遇到下面錯誤

Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.9.0.00040)
Cortex_M4_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.9.0.00040)
Cortex_M4_0: Unable to determine target status after 20 attempts
Cortex_M4_0: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging