This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541的RF负载阻抗值

Other Parts Discussed in Thread: CC2541

通常在电路图上,会标注一些RF阻抗线的class,例如50Ω、100Ω,目的是规定厂家做PCB时控制好高频走线的阻抗。对CC2541这颗2.4G蓝牙器件而言,根据其spec,有一对差分RF信号线的最佳负载阻抗为70+j30Ω。是否只要把这一对差分阻抗线按常规标注成70Ω即可?虚部j30怎样对待?求确认。

  • 你好,这里其实有微波技术中的两个概念,一个馈线是微带线/或带状线的特征阻抗,另外一个是最佳负载/天线的阻抗匹配.

    因此在这里你需要做的是阻抗匹配.简单说来建议用矢量网络分析仪来调整阻抗以达到最佳输出匹配使信号完成最大效率的传输.

  • Hi Robin,

    我的意思是这个做法是否正确:电路图中按常规将差分线标注一下class为70Ω,然后PCB厂家在做板子时就会按这个阻抗值去做,以此来保证传输线阻抗符合spec要求。

    所以我的问题重点是传输线取这个70Ω的数值是否合适。因为之前常见的RF电路一般都是单端要求50欧姆阻抗或差分线100欧姆,没有见到过spec标明70Ω+j30这种后面还加上虚部的要求,因此需要确认一下制作PCB板子的传输线该如何确定其阻抗值。至于匹配电路的调试在画图阶段先不考虑,可以在板子拿到手后再说。

    谢谢。

  • 你好.有关layout建议你先看下面这篇文章,谢谢

    • AN098 - Layout Review Techniques for Low Power RF Designs (Rev. A) 

    http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=swra367a&fileType=pdf

  • 谢谢你的提示,这个早就看过了,没有找到答案。其实只是想确认一下这一对PCB传输线的阻抗是否要做70Ω,这种规格的东西以前没用过,所以才要咨询一下,如果是50\100Ω的线也不用专门提case了嘛。

  • 这样不行, 一般来说PCB厂商无法准确控制复数阻抗。最佳方法是完全按照 TI 的参考设计的布板来走线和选择叠层结构。

  • 谢谢回复。完全follow参考设计有一定困难,主要原因还是布板面积不够用。一方面我们会尽量按参考设计布板,另一方面也会去咨询PCB板厂的工艺能否达到比较精确的70+j30Ω的复数阻抗要求,如果达不到只能是尽量减小偏差,然后板子拿到后通过调匹配使之靠近spec要求。