This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2540在ADC转化时的问题。



请问一个关于ADC转化的问题:

我在VCC与P0_1之间接了一个30k的电阻,在P0_1和GND之间接了一个30K的电阻。

代码为:

P0SEL = P0SEL | 0x02;

P0DIR = 0xFD;  

P0 = 0x00;

v_1 = HalAdcRead(HAL_ADC_CHANNEL_1, HAL_ADC_RESOLUTION_12);

最后测得的值显示这两个电阻的比值不为1,请问这是怎么回事。

  • adc需要参考源,默认是如下:

    #define HAL_ADC_REF_VOLT    HAL_ADC_REF_AVDD 参考源是AVDD

    adcRef = HAL_ADC_REF_VOLT;

    不是很准确,会变化。建议使用内部的1.25V作为参考源HAL_ADC_REF_125V

    这时,并且分压值要保证小于1.25V,比如一个60K,一个30K