请教TI 工程师,
我使用CC2541 BLE协议栈 中 simpleBLEBroadcaster ,想更改该名称,
在simpleBLEBroadcaster.c文件中增加如下代码:
static uint8 attDeviceName[GAP_DEVICE_NAME_LEN] = "HT15TTTTT";
在函数:void SimpleBLEBroadcaster_Init( uint8 task_id ) 增加:
// 设置GAP特性 Set the GAP Characteristics 改名字
uint8 devNamePermission = GATT_PERMIT_READ | GATT_PERMIT_WRITE;
GGS_SetParameter(GGS_W_PERMIT_DEVICE_NAME_ATT, sizeof(uint8), &devNamePermission);
GGS_SetParameter( GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN+1, attDeviceName );
//上面是新增加的//////////////////////////////////////////////////////////////////////////////////
编译出现如下错误:
Error[e46]: Undefined external "gapServiceUUID" referred in gapgattserver ( E:\work\MSPBLEindependent\ble\Projects\ble\Libraries\CC2541DB\bin\CC2541_BLE_bcast.lib )
Error[e46]: Undefined external "primaryServiceUUID" referred in gapgattserver ( E:\work\MSPBLEindependent\ble\Projects\ble\Libraries\CC2541DB\bin\CC2541_BLE_bcast.lib )
Error[e46]: Undefined external "characterUUID" referred in gapgattserver ( E:\work\MSPBLEindependent\ble\Projects\ble\Libraries\CC2541DB\bin\CC2541_BLE_bcast.lib )
Error[e46]: Undefined external "deviceNameUUID" referred in gapgattserver ( E:\work\MSPBLEindependent\ble\Projects\ble\Libraries\CC2541DB\bin\CC2541_BLE_bcast.lib )
Error[e46]: Undefined external "appearanceUUID" referred in gapgattserver ( E:\work\MSPBLEindependent\ble\Projects\ble\Libraries\CC2541DB\bin\CC2541_BLE_bcast.lib )
不知是什么问题? 谢谢!
TAN
如下是simpleBLEBroadcaster.c
#include "bcomdef.h"
#include "OSAL.h"
#include "OSAL_PwrMgr.h"
#include "OnBoard.h"
#include "hal_adc.h"
#include "hal_led.h"
#include "hal_key.h"
#include "hal_lcd.h"
#include "hci.h"
#include "gap.h"
#include "devinfoservice.h"
#include "broadcaster.h"
#include "simpleBLEBroadcaster.h"
#include "gapgattserver.h"
//增加下面的#include
#include "gatt.h"
#include "gattservapp.h"
#include "simpleGATTprofile.h"
//上面是新增加的
/*********************************************************************
* MACROS
*/
/*********************************************************************
* CONSTANTS
*/
// What is the advertising interval when device is discoverable (units of 625us, 160=100ms)
#define DEFAULT_ADVERTISING_INTERVAL 160
// Company Identifier: Texas Instruments Inc. (13)
#define TI_COMPANY_ID 0x000D
// Length of bd addr as a string
#define B_ADDR_STR_LEN 15
/*********************************************************************
* TYPEDEFS
*/
/*********************************************************************
* GLOBAL VARIABLES
*/
/*********************************************************************
* EXTERNAL VARIABLES
*/
/*********************************************************************
* EXTERNAL FUNCTIONS
*/
/*********************************************************************
* LOCAL VARIABLES
*/
static uint8 simpleBLEBroadcaster_TaskID; // Task ID for internal task/event processing
/*集中器设备可以通过扫描来发现正在发送广告数据的节点设备,当节点设备接收到集中器设备的扫描请求后,回应的数据内容如下:*/
// GAP - SCAN RSP data (max size = 31 bytes)
static uint8 scanRspData[] =
{
// complete name
0x15, // length of this data
GAP_ADTYPE_LOCAL_NAME_COMPLETE, //0x09 !< Complete local name
0x53, // 'S'
0x69, // 'i'
0x6d, // 'm'
0x70, // 'p'
0x6c, // 'l'
0x65, // 'e'
0x42, // 'B'
0x4c, // 'L'
0x45, // 'E'
0x42, // 'B'
0x72, // 'r'
0x6f, // 'o'
0x61, // 'a'
0x64, // 'd'
0x63, // 'c'
0x61, // 'a'
0x73, // 's'
0x74, // 't'
0x65, // 'e'
0x72, // 'r'
// Tx power level
0x02, // length of this data
GAP_ADTYPE_POWER_LEVEL, //指明接下来的数据为发射功率,发射功率的可调范围为:-127~127dbm
0 // 将发射功率设置为:0dBm
};
// GAP - Advertisement data (max size = 31 bytes, though this is
// best kept short to conserve power while advertisting)
static uint8 advertData[] =
{
// Flags; this sets the device to use limited discoverable
// mode (advertises for 30 seconds at a time) instead of general
// discoverable mode (advertises indefinitely)
0x02, // length of this data
GAP_ADTYPE_FLAGS,
GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,
// three-byte broadcast of the data "1 2 3"
0x04, // length of this data including the data type byte
GAP_ADTYPE_MANUFACTURER_SPECIFIC, // manufacturer specific advertisement data type
1,
2,
3
/*
//设置可发现模式,不支持传统蓝牙
0x02, //广告中设置发现模式的数据段,占用2个字节数据长度
GAP_ADTYPE_FLAGS, //01 广告类型标志:!< Discovery Mode: @ref GAP_ADTYPE_FLAGS_MODES
0x1A, //定义节点设备的可发现模式
0x1A, //广告中设置 GAP基本服务UUID的数据段,占用3字节数据长度
GAP_ADTYPE_MANUFACTURER_SPECIFIC, //!< Manufacturer Specific Data: first 2 octets contain the Company Identifier Code followed by the additional manufacturer specific data
// 部分服务 UUID
0x4C,
0x00,
0x02,
0x15,
0xD5,//D0 //北京试点第二批
0xC5,
0x6D,
0xB5,
0xDF,
0xFB,
0x48,
0xD2,
0xB0,
0x60,
0xD0,
0xF5,
0xA7,
0x10,
0x96,
0xE0, ////
0x00,
0x00,
0x00,
0x00,
0xC5
*/
};
/*add*/
// GAP设备名字 GAP GATT Attributes
static uint8 attDeviceName[GAP_DEVICE_NAME_LEN] = "HT15TTTTT";
/*********************************************************************
* LOCAL FUNCTIONS
*/
static void simpleBLEBroadcaster_ProcessOSALMsg( osal_event_hdr_t *pMsg );
static void peripheralStateNotificationCB( gaprole_States_t newState );
#if defined( CC2540_MINIDK )
static void simpleBLEBroadcaster_HandleKeys( uint8 shift, uint8 keys );
#endif
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
static char *bdAddr2Str ( uint8 *pAddr );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
/*********************************************************************
* PROFILE CALLBACKS
*/
// GAP Role Callbacks
static gapRolesCBs_t simpleBLEBroadcaster_BroadcasterCBs =
{
peripheralStateNotificationCB, // Profile State Change Callbacks
NULL // When a valid RSSI is read from controller (not used by application)
};
/*********************************************************************
* PUBLIC FUNCTIONS
*/
/*********************************************************************
* @fn SimpleBLEBroadcaster_Init
*
* @brief Initialization function for the Simple BLE Broadcaster App
* Task. This is called during initialization and should contain
* any application specific initialization (ie. hardware
* initialization/setup, table initialization, power up
* notificaiton ... ).
*
* @param task_id - the ID assigned by OSAL. This ID should be
* used to send messages and set timers.
*
* @return none
*/
void SimpleBLEBroadcaster_Init( uint8 task_id )
{
simpleBLEBroadcaster_TaskID = task_id;
// Setup the GAP Broadcaster Role Profile
{
#if defined( CC2540_MINIDK )
// For the CC2540DK-MINI keyfob, device doesn't start advertising until button is pressed
uint8 initial_advertising_enable = FALSE;
#else
// For other hardware platforms, device starts advertising upon initialization
uint8 initial_advertising_enable = TRUE;
#endif
// By setting this to zero, the device will go into the waiting state after
// being discoverable for 30.72 second, and will not being advertising again
// until the enabler is set back to TRUE
uint16 gapRole_AdvertOffTime = 0;
uint8 advType = GAP_ADTYPE_ADV_NONCONN_IND; // use non-connectable advertisements
// uint8 advType = GAP_ADTYPE_ADV_DISCOVER_IND; // use scannable unidirected advertisements
// Set the GAP Role Parameters
GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8 ), &initial_advertising_enable );
GAPRole_SetParameter( GAPROLE_ADVERT_OFF_TIME, sizeof( uint16 ), &gapRole_AdvertOffTime );
GAPRole_SetParameter( GAPROLE_SCAN_RSP_DATA, sizeof ( scanRspData ), scanRspData );
GAPRole_SetParameter( GAPROLE_ADVERT_DATA, sizeof( advertData ), advertData );
GAPRole_SetParameter( GAPROLE_ADV_EVENT_TYPE, sizeof( uint8 ), &advType );
}
// 设置GAP特性 Set the GAP Characteristics 改名字
uint8 devNamePermission = GATT_PERMIT_READ | GATT_PERMIT_WRITE;
GGS_SetParameter(GGS_W_PERMIT_DEVICE_NAME_ATT, sizeof(uint8), &devNamePermission);
GGS_SetParameter( GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN+1, attDeviceName );
//上面是新增加的//////////////////////////////////////////////////////////////////////////////////
// Set advertising interval
{
uint16 advInt = DEFAULT_ADVERTISING_INTERVAL;
GAP_SetParamValue( TGAP_LIM_DISC_ADV_INT_MIN, advInt );
GAP_SetParamValue( TGAP_LIM_DISC_ADV_INT_MAX, advInt );
GAP_SetParamValue( TGAP_GEN_DISC_ADV_INT_MIN, advInt );
GAP_SetParamValue( TGAP_GEN_DISC_ADV_INT_MAX, advInt );
}
#if defined( CC2540_MINIDK )
// Register for all key events - This app will handle all key events
RegisterForKeys( simpleBLEBroadcaster_TaskID );
// makes sure LEDs are off
HalLedSet( (HAL_LED_1 | HAL_LED_2), HAL_LED_MODE_OFF );
// For keyfob board set GPIO pins into a power-optimized state
// Note that there is still some leakage current from the buzzer,
// accelerometer, LEDs, and buttons on the PCB.
P0SEL = 0; // Configure Port 0 as GPIO
P1SEL = 0; // Configure Port 1 as GPIO
P2SEL = 0; // Configure Port 2 as GPIO
P0DIR = 0xFC; // Port 0 pins P0.0 and P0.1 as input (buttons),
// all others (P0.2-P0.7) as output
P1DIR = 0xFF; // All port 1 pins (P1.0-P1.7) as output
P2DIR = 0x1F; // All port 1 pins (P2.0-P2.4) as output
P0 = 0x03; // All pins on port 0 to low except for P0.0 and P0.1 (buttons)
P1 = 0; // All pins on port 1 to low
P2 = 0; // All pins on port 2 to low
#endif // #if defined( CC2540_MINIDK )
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
HalLcdWriteString( "BLE Broadcaster", HAL_LCD_LINE_1 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
// Setup a delayed profile startup
osal_set_event( simpleBLEBroadcaster_TaskID, SBP_START_DEVICE_EVT );
}
/*********************************************************************
* @fn SimpleBLEBroadcaster_ProcessEvent
*
* @brief Simple BLE Broadcaster Application Task event processor. This
* function is called to process all events for the task. Events
* include timers, messages and any other user defined events.
*
* @param task_id - The OSAL assigned task ID.
* @param events - events to process. This is a bit map and can
* contain more than one event.
*
* @return events not processed
*/
uint16 SimpleBLEBroadcaster_ProcessEvent( uint8 task_id, uint16 events )
{
VOID task_id; // OSAL required parameter that isn't used in this function
if ( events & SYS_EVENT_MSG )
{
uint8 *pMsg;
if ( (pMsg = osal_msg_receive( simpleBLEBroadcaster_TaskID )) != NULL )
{
simpleBLEBroadcaster_ProcessOSALMsg( (osal_event_hdr_t *)pMsg );
// Release the OSAL message
VOID osal_msg_deallocate( pMsg );
}
// return unprocessed events
return (events ^ SYS_EVENT_MSG);
}
if ( events & SBP_START_DEVICE_EVT )
{
// Start the Device
VOID GAPRole_StartDevice( &simpleBLEBroadcaster_BroadcasterCBs );
return ( events ^ SBP_START_DEVICE_EVT );
}
// Discard unknown events
return 0;
}
/*********************************************************************
* @fn simpleBLEBroadcaster_ProcessOSALMsg
*
* @brief Process an incoming task message.
*
* @param pMsg - message to process
*
* @return none
*/
static void simpleBLEBroadcaster_ProcessOSALMsg( osal_event_hdr_t *pMsg )
{
switch ( pMsg->event )
{
#if defined( CC2540_MINIDK )
case KEY_CHANGE:
simpleBLEBroadcaster_HandleKeys( ((keyChange_t *)pMsg)->state, ((keyChange_t *)pMsg)->keys );
break;
#endif // CC2540_MINIDK
default:
// do nothing
break;
}
}
#if defined( CC2540_MINIDK )
/*********************************************************************
* @fn simpleBLEBroadcaster_HandleKeys
*
* @brief Handles all key events for this device.
*
* @param shift - true if in shift/alt.
* @param keys - bit field for key events. Valid entries:
* HAL_KEY_SW_2
* HAL_KEY_SW_1
*
* @return none
*/
static void simpleBLEBroadcaster_HandleKeys( uint8 shift, uint8 keys )
{
VOID shift; // Intentionally unreferenced parameter
if ( keys & HAL_KEY_SW_2 )
{
// ressing the right key should toggle advertising on and off
uint8 current_adv_enabled_status;
uint8 new_adv_enabled_status;
//Find the current GAP advertisement status
GAPRole_GetParameter( GAPROLE_ADVERT_ENABLED, ¤t_adv_enabled_status );
if( current_adv_enabled_status == FALSE )
{
new_adv_enabled_status = TRUE;
}
else
{
new_adv_enabled_status = FALSE;
}
//change the GAP advertisement status to opposite of current status
GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8 ), &new_adv_enabled_status );
}
}
#endif // CC2540_MINIDK
/*********************************************************************
* @fn peripheralStateNotificationCB
*
* @brief Notification from the profile of a state change.
*
* @param newState - new state
*
* @return none
*/
static void peripheralStateNotificationCB( gaprole_States_t newState )
{
switch ( newState )
{
case GAPROLE_STARTED:
{
uint8 ownAddress[B_ADDR_LEN];
GAPRole_GetParameter(GAPROLE_BD_ADDR, ownAddress);
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
// Display device address
HalLcdWriteString( bdAddr2Str( ownAddress ), HAL_LCD_LINE_2 );
HalLcdWriteString( "Initialized", HAL_LCD_LINE_3 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
}
break;
case GAPROLE_ADVERTISING:
{
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
HalLcdWriteString( "Advertising", HAL_LCD_LINE_3 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
}
break;
case GAPROLE_WAITING:
{
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
HalLcdWriteString( "Waiting", HAL_LCD_LINE_3 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
}
break;
case GAPROLE_ERROR:
{
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
HalLcdWriteString( "Error", HAL_LCD_LINE_3 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
}
break;
default:
{
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
HalLcdWriteString( "", HAL_LCD_LINE_3 );
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
}
break;
}
}
#if (defined HAL_LCD) && (HAL_LCD == TRUE)
/*********************************************************************
* @fn bdAddr2Str
*
* @brief Convert Bluetooth address to string. Only needed when
* LCD display is used.
*
* @return none
*/
char *bdAddr2Str( uint8 *pAddr )
{
uint8 i;
char hex[] = "0123456789ABCDEF";
static char str[B_ADDR_STR_LEN];
char *pStr = str;
*pStr++ = '0';
*pStr++ = 'x';
// Start from end of addr
pAddr += B_ADDR_LEN;
for ( i = B_ADDR_LEN; i > 0; i-- )
{
*pStr++ = hex[*--pAddr >> 4];
*pStr++ = hex[*pAddr & 0x0F];
}
*pStr = 0;
return str;
}
#endif // (defined HAL_LCD) && (HAL_LCD == TRUE)
/*********************************************************************
*********************************************************************/