This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一个关于ADC转化的问题:
我在VCC与P0_1之间接了一个30k的电阻,在P0_1和GND之间接了一个30K的电阻。
代码为:
P0SEL = P0SEL | 0x02;
P0DIR = 0xFD;
P0 = 0x00;
v_1 = HalAdcRead(HAL_ADC_CHANNEL_1, HAL_ADC_RESOLUTION_12);
最后测得的值显示这两个电阻的比值不为1,请问这是怎么回事。