请问各位:
cc2540 做为Central角色连接上了外围设备,之后连接断开,会返回 pEvent->linkTerminate.reason,表示原因的参数,请问关于terminate reason参数的说明在哪里可以找到啊?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
/*
** LL API Status Codes
**
** Note: These status values map directly to the HCI Error Codes.
** Per the Bluetooth Core Specification, V4.0.0, Vol. 2, Part D.
*/
#define LL_STATUS_SUCCESS 0x00 // Success
#define LL_STATUS_ERROR_UNKNOWN_CONN_HANDLE 0x02 // Unknown Connection Identifier
#define LL_STATUS_ERROR_INACTIVE_CONNECTION 0x02 // Unknown Connection Identifier for now; may be needed for multiple connections
#define LL_STATUS_ERROR_AUTH_FAILURE 0x05 // Authentication Failure
#define LL_STATUS_ERROR_PIN_OR_KEY_MISSING 0x06 // Pin or Key Missing
#define LL_STATUS_ERROR_OUT_OF_CONN_RESOURCES 0x07 // Memory Capacity Exceeded
#define LL_STATUS_ERROR_OUT_OF_TX_MEM 0x07 // Memory Capacity Exceeded
#define LL_STATUS_ERROR_OUT_OF_RX_MEM 0x07 // Memory Capacity Exceeded
#define LL_STATUS_ERROR_OUT_OF_HEAP 0x07 // Memory Capacity Exceeded
#define LL_STATUS_ERROR_WL_TABLE_FULL 0x07 // Memory Capacity Exceeded
#define LL_STATUS_ERROR_CONNECTION_TIMEOUT 0x08 // Connection Timeout
#define LL_STATUS_ERROR_CONNECTION_LIMIT_EXCEEDED 0x09 // Connection Limit Exceeded
#define LL_STATUS_ERROR_COMMAND_DISALLOWED 0x0C // Command Disallowed
#define LL_STATUS_ERROR_DUE_TO_LIMITED_RESOURCES 0x0D // Command Rejected Due To Limited Resources
#define LL_STATUS_ERROR_DUE_TO_DELAYED_RESOURCES 0x0D // Command Delayed Due To Limited Resources
#define LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED 0x11 // Unsupported Feature or Parameter Value
#define LL_STATUS_ERROR_UNEXPECTED_PARAMETER 0x12 // Invalid HCI Command Parameters
#define LL_STATUS_ERROR_ILLEGAL_PARAM_COMBINATION 0x12 // Invalid HCI Command Parameters
#define LL_STATUS_ERROR_BAD_PARAMETER 0x12 // Invalid HCI Command Parameters or 0x30: Parameter Out of Mandatory Range?
#define LL_STATUS_ERROR_UNKNOWN_ADV_EVT_TYPE 0x12 // Invalid HCI Command Parameters or 0x30: Parameter Out of Mandatory Range?
#define LL_STATUS_ERROR_PEER_TERM 0x13 // Remote User Terminated Connection
#define LL_STATUS_ERROR_PEER_DEVICE_TERM_LOW_RESOURCES 0x14 // Remote Device Terminated Connection Due To Low Resources
#define LL_STATUS_ERROR_PEER_DEVICE_TERM_POWER_OFF 0x15 // Remote Device Terminated Connection Due To Power Off
#define LL_STATUS_ERROR_HOST_TERM 0x16 // Connection Terminated By Local Host
#define LL_STATUS_ERROR_UNSUPPORTED_REMOTE_FEATURE 0x1A // Unsupported Remote Feature
#define LL_STATUS_ERROR_WL_ENTRY_NOT_FOUND 0x1F // Unspecified Error
#define LL_STATUS_ERROR_WL_TABLE_EMPTY 0x1F // Unspecified Error
#define LL_STATUS_ERROR_RNG_FAILURE 0x1F // Unspecified Error
#define LL_STATUS_ERROR_DISCONNECT_IMMEDIATE 0x1F // Unspecified Error
#define LL_STATUS_ERROR_UNEXPECTED_STATE_ROLE 0x21 // Role Change Not Allowed
#define LL_STATUS_ERROR_LL_TIMEOUT 0x22 // Link Layer Response Timeout
#define LL_STATUS_ERROR_LL_TIMEOUT_HOST 0x22 // Link Layer Response Timeout
#define LL_STATUS_ERROR_LL_TIMEOUT_PEER 0x22 // Link Layer Response Timeout
#define LL_STATUS_ERROR_INSTANT_PASSED 0x28 // Instant Passed
#define LL_STATUS_ERROR_INSTANT_PASSED_HOST 0x28 // Instant Passed
#define LL_STATUS_ERROR_INSTANT_PASSED_PEER 0x28 // Instant Passed
#define LL_STATUS_ERROR_KEY_PAIRING_NOT_SUPPORTED 0x29 // Pairing With Unit Key Not Supported
#define LL_STATUS_ERROR_NO_ADV_CHAN_FOUND 0x30 // Parameter Out Of Mandatory Range
#define LL_STATUS_ERROR_PARAM_OUT_OF_RANGE 0x30 // Parameter Out Of Mandatory Range
#define LL_STATUS_ERROR_UPDATE_CTRL_PROC_PENDING 0x3A // Controller Busy
#define LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE 0x3A // Controller Busy
#define LL_STATUS_ERROR_VER_INFO_REQ_ALREADY_PENDING 0x3A // Controller Busy
#define LL_STATUS_ERROR_UNACCEPTABLE_CONN_INTERVAL 0x3B // Unacceptable Connection Interval
#define LL_STATUS_ERROR_DIRECTED_ADV_TIMEOUT 0x3C // Directed Advertising Timeout
#define LL_STATUS_ERROR_CONN_TERM_DUE_TO_MIC_FAILURE 0x3D // Connection Terminated Due To MIC Failure
#define LL_STATUS_ERROR_CONN_FAILED_TO_BE_ESTABLISHED 0x3E // Connection Failed To Be Established
#define LL_STATUS_ERROR_CONN_TIMING_FAILURE 0x3F // MAC Connection Failed