dear all:
我的设置MIN_INTERVAL=16(20ms)。MAX _MAX_INTERVAL=32(40ms) PARAM_UPDATE=TRUE
用light建立连接后发现INTERVAL是40ms。
请问可以和ios设备建立20ms interval的连接吗?如果可以,参数如何设置啊?
BR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.