Other Parts Discussed in Thread: CC2540
Error[e16]: Segment ISTACK (size: 0xc0 align: 0) is too long for segment definition. At least 0x7 more bytes needed. The problem occurred while processing the segment
placement command "-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#08-_IDATA_END", where at the moment of placement the available memory ranges were "IDATA:47-ff"
Reserved ranges relevant to this placement:
IDATA:8-1f VREG
IDATA:21-3f VREG
IDATA:40-41 XSP
IDATA:42-42 DATA_I
IDATA:43-44 DATA_Z
IDATA:45-46 IDATA_Z
IDATA:47-ff ISTACK
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:e8-ef SFR_AN
BIT:f8-ff SFR_AN
Error while running Linker