This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用芯片CC2541,想问下,可以通过管脚输出32768HZ吗?
Hi min,
不可以。无论哪个timer都做不到。
有的mcu可以直接把时钟信号输出,不知道CC2541可以不可以直接通过管脚把时钟信号输出。
Hi Min,
CC2451没有专门的时钟输出管脚,你可以考虑根据你的应用从其他的MCU中输出32.768KHZ的信号。
在我们的典型设计中,一般会通过类似MSP430的产品将32.768KHZ的信号输出给CC2541。
谢谢
ken
谢谢!我的应用很简单,不想加入MCU,就是把一个传感器的数据读出,通过蓝牙发出,传感器是I2C接口的,主要是传感器要输入一个32.768KHZ的脉冲信号,如果cc2541不能输出,我考虑增加一个有源晶振,或者增加个可以输出32.768khz的RTC.
明白你的需求。确实你外加一个32.768Khz的晶振回来的更快更方便实现你所需的功能。