以TI公司的CC2540为例,它支持4种发射功率选择:4dBm、0dBm、-6dBm和-23dBm,按无线电功率定义:LdBm=10lg(Pwr/1mW),以上4种分贝值换算成瓦特为:2.51mW、1mW、0.251mW和0.005mW,有效通信距离分别为:30米、10米、7米和3米。
如何在BLE 中设定外设或集中器的发射功率呢? 默认值是多少?在哪里可以找到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
以TI公司的CC2540为例,它支持4种发射功率选择:4dBm、0dBm、-6dBm和-23dBm,按无线电功率定义:LdBm=10lg(Pwr/1mW),以上4种分贝值换算成瓦特为:2.51mW、1mW、0.251mW和0.005mW,有效通信距离分别为:30米、10米、7米和3米。
如何在BLE 中设定外设或集中器的发射功率呢? 默认值是多少?在哪里可以找到
/*******************************************************************************
* @fn HCI_EXT_SetTxPowerCmd API
*
* @brief This HCI Extension API is used to set the transmit power.
*
* Related Events: HCI_VendorSpecifcCommandCompleteEvent
*
* input parameters
*
* @param txPower - LL_EXT_TX_POWER_MINUS_23_DBM,
* LL_EXT_TX_POWER_MINUS_6_DBM,
* LL_EXT_TX_POWER_0_DBM,
* LL_EXT_TX_POWER_4_DBM
*
* output parameters
*
* @param None.
*
* @return hciStatus_t
*/
extern hciStatus_t HCI_EXT_SetTxPowerCmd( uint8 txPower );