This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540低功耗处理

Other Parts Discussed in Thread: CC2540

大家好!

        我的CC2540工作在主模式下,现在在做CC2540低功耗处理这一块,在在IAR中打开了POWER_SAVING,同时也关闭了xHAL_LCD=TRUE、xHAL_UART=TRUE,系统上电后,是可以正常进入低功耗状态的,但是经过我的测量(未连接状态下),电流为200uA左右。在连接状态下(不进行数据发送)的电流为2.5mA左右,在有数据发送状态下,电流为3.5mA左右。我感觉电流还是很大,想进一步的降低功耗,不知道该如何处理?

        另外,我分析了工程代码,发现CC2540的低功耗处理是由OSAL自动进行处理的,而且UART采用的是轮询的方式,如果在IAR中打开了HAL_UART=TRUE宏,系统是不会进入低功耗状态的。我现在想系统即可以进入低功耗,而且UART也能正常工作,该如何处理呢?

        可否将默认的UART改为中断触发的方式呢?