This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R-Q1: CC2642的Continuous TX/RX和Packet TX/RX测试

Part Number: CC2642R-Q1

想使用smartRF studio做CC2642的Continuous TX/RX和Packet TX/RX测试,在PC上使用XDS100V3接入两块板子(都是CC2642的芯片)后,smartRF studio的主窗口中只能识别出一个如图一所示

图一

并且在打开device control panel时只能打开一个,如果再打开一个smartRF studio的话会识别出一个XDS device ID相同的CC2642,再打开device control panel时会出现如图二的信息

图二

想问问这到底是什么情况,或者如何才能进行在同一个PC上做CC2642的Continuous TX/RX和Packet TX/RX测试