This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: 断开连接之后,设置广播间隔、调用打开广播接口,实际广播没打开

Part Number: CC2642R


执行断开事件GAP_LINK_TERMINATED_EVENT时,调用下面接口设置广播间隔和打开广播
      uint16_t advInterval = 160;
      GapAdv_setParam(advHandle, GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, &advInterval);
      GapAdv_setParam(advHandle, GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX, &advInterval);
      GapAdv_enable(advHandle, GAP_ADV_ENABLE_OPTIONS_USE_MAX , 0);
可以收到GAP_EVT_ADV_START_AFTER_ENABLE事件,但是实际没有广播成功,用抓包器抓不到广播,GPIO监控 RF状态也是失败


工程使用 simple_peripheral_oad_onchip 改的,SDK版本是simplelink_cc13x2_26x2_sdk_5_20_00_52