This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2564的蓝牙3.0 SPP传输速率是多少呢?

1)最大支持波特率是多少?

2)是双向都同时支持以最大波特率传输吗?

3)2.1+EDR(3 Mbits/s)能支持115200波特率,蓝牙3.0(24 Mbit/s)是 2.1+EDR的8倍 ,是不是可以支持921600波特率呢?

----------------------

假设最高波特率为115200,数据位为8bit,起始位为1bit,结束位为1bit,校验位为1bit;
那1s钟不间断可传送的字符(1bit起始位+8bit数据位+1bit校验位+1bit结束位,共11bit)为115200/11=10472;速率约为10kB/ps;
传送一幅200KB的图片,需要的时间约为20s;

  • yu,

    1. 2564的UART接口最大支持波特率为3M。如果你说的是空中的SPP 蓝牙profile的速度,这个跟物理的UART有点不太一样,没有波特率概念,只能以蓝牙的实际速度来表示,你可以理解为3Mbps。

    2. 理论上可以同时传数据,但是总的带宽不会变,因此照此推算的话应该是一半一半。

    3. 由于没有波特率概念,完全取决于蓝牙芯片的实际传输速度。