Other Parts Discussed in Thread: CC2541, TPS62730
你好,ti介绍用tps67232与CC2541结合会更省功耗,所以我采纳了TI的建议,加上了这个旁压转换器,原来的keyfob是用P0.7控制tps67232工作的,而我的电路板是用P1.6的,所以我将keyfob原代码中的P0_7口改成P1.6口控制TPS67232
#if defined ( DC_DC_P0_7 )
// Enable stack to toggle bypass control on TPS62730 (DC/DC converter)
HCI_EXT_MapPmIoPortCmd( HCI_EXT_PM_IO_PORT_P1, HCI_EXT_PM_IO_PORT_PIN6 );
#endif // defined ( DC_DC_P0_7 )
但是发现测出的电池电量是25%,也就是测电压是tps67232是处于工作模式的,这是为什么呢?
上面这个函数HCI_EXT_MapPmIoPortCmd有一句解释是“The GPIO output will be High on Wake, and Low upon entering Sleep.”也就是说这个函数会控制tps67232工作,降低功耗,实际测试功耗是降了,但测出的电压时25%左右,我觉得是我测电压时tps67232还处于工作模式,测的还是2.2V那个电压,而不是外部的3V电压,希望YAN,VIKI可以帮忙看看,搞了几天都没头绪。。。